About Recordings
The 89600 VSA software can record time data from measurement hardware directly to a PC's disk drive. The data can be played back at a later time or imported into other applications. Recordings can also be created in a different program and the recording used in the VSA.
The Recording and Playback feature is not available with Power Spectrum measurements.
The following is a list of topics about working with recordings:
- Creating a Recording
- Creating a Recording Using an ASCII Editor
- Playing a Recording
- Saving a Recording
- Recalling a Recording
- Recalling Multiple Single-Channel Recordings
- Using the Record Player
- Record Data File Formats
- Recording dialog box parameters
Recording Block Diagram
The following block diagram is a portion of that shown in the VSA Block Diagram. It shows how recording fits into the overall VSA block diagram.
Example recordings
Example recordings are included with the 89600 VSA software. The recordings are located in this directory.
%PROGRAMFILES%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software
Each recording has a corresponding setup file and a signal description. See Recalling a Signal Demo for more information.
See Demo's and Recorded Signals for a list and descriptions of the available recordings.
See Also