Saving and Recalling Recordings
Sharing Data With Other Applications

The 89600 VSA software lets you record time data from your measurement hardware directly to your PC's disk drive. You can play the data back at a later time or import it into other applications. You can also create and play your own recording. To learn about recordings (including: Creating, Playing, Saving, Recalling and using the Player), see the About Recordings topic in the Reference > Recordings book.

When you use the VSA to create a recording, the Input Channel configuration determines how many channels that the recording captures data from [click Input > Channels].

To recall a multi-channel recording when you do not have real hardware with enough channels, you can use Simulated Hardware.

File Structure

All recording files contain a header and one or more arrays of captured data. The header contains a list of variables that describe the recording. For information about the data header and the individual header variables, see About the Data Header.

The header in a recording file contains some of the same variable found in a trace file. To see the header variables used in a recording file, follow these steps:

  1. Save the recording as an ASCII file (*.txt or *.csv). See Saving a Recording for details.
  2. View the recording file with an ASCII editor.

Supported File Formats

You can save recordings in any of the formats listed in Supported File Formats.