Demodulation Multi-Measurement Setup

To configure the VSA to perform modulation analysis:

  1. Select the measurement that you want to configure (select the active measurement in a multi-measurement configuration).

    From the measurements dropdown list on the VSA toolbar, select the desired measurement.

  2. Select the demodulator by clicking Analysis > Type and choose the desired demodulator from the list.

  3. Configure the demodulator parameters.

    Each demodulator has a unique set of associated properties accessed by clicking Analysis > {demodulator name} Properties.

    Each demodulator documentation includes a Setting up a Measurement topic which can be accessed from the Measurement Setup book in the Table of Contents for that measurement type.

    See Selecting a Measurement Type for a list of links to the documentation for each measurement type.

See Also

Selecting a Measurement Type

Configuring Multiple Measurements