Trace Tab (Display Preferences)
The
tab on the menu turns on and off the display grids, annotation, and to choose to display all frequency points. The default setting is checked for grids and annotation and cleared for display all frequency points.Trace Decoration
-
: When is cleared, the grid lines in the trace windows are removed.
-
: When is cleared, all the trace annotation is removed and the trace grid expands accordingly.
Trace Layout
-
Preset Setup or Preset Traces.
: specifies the minimum number of trace windows that exist after aWhen the current set of traces contains fewer trace windows than the Minimum Trace Count, the remaining traces will not be visible but will be present in the list of traces, which is shown at the top of the tabs in the
dialog box ( , for example). -
Preset Setup or Preset Traces, down to the minimum number specified by .
: When selected, the VSA removes any traces that are no longer visible after a -
Tile Visible operation after you perform a Preset Setup.
: When selected, the VSA performs a -
Preset Traces is performed when you select a different input channel configuration.
: When selected, a -
Trace Window. Otherwise, the VSA places the new measurement's traces into the current window.
: When selected, the VSA places the default traces for a newly created measurement into a new
Miscellaneous
-
: When is cleared, only alias-protected data is shown. When is selected, all data including aliased frequency points is shown. This also includes data that extends beyond the measurement hardware’s minimum or maximum frequency range. The data that is shown may not be valid, so use caution when using this setting.
See Understanding Time and Frequency parameters for more information.
-
: Enabling this parameter will "sample and hold" (show point value for duration of bin) for each point instead of the default linear interpolation between points.
See Also