Preset Traces
Clicking will reset the trace layout for the specified measurement to the default set of traces for the currently selected measurement type.
Each measurement type has a initial set of traces. The default set of traces can be affected by how many input channels are configured.
In addition, when there are multiple Trace Windows, the traces for the preset measurement will be collected into the window in which the menu item was selected. After the traces are collected, the traces will be Tiled within the window.
only affects traces. Any other types of windows (Markers, Macros, etc.) are left in their current position.
See Also