Analyzer Calibration Dialog
is used to run a calibration that is implemented in the analyzer hardware. (e.g., alignments in an X-Series analyzer). Analyzer Calibration affects the data that VSA reads from the analyzer, but does not change anything in VSA data processing or analysis.
Not all analyzers support this feature.
- Last Calibration: Provides the time that the last calibration was performed.
- Calibrate: Performs a single calibration procedure.
- Quick Cal: Initiates a smart calibration procedure. (Applies to Keysight X-Series Signal Analyzers only.)
- Single Cal: Initiates a full calibration procedure which may take several minutes.
- Auto Calibrate: Calibration status is monitored and is performed when a calibration is needed. (Applies to Keysight X-Series Signal Analyzers only.)
- Calibration Mode: Affects when VSA indicates a calibration needed.
- Calibration Mode Auto: VSA uses the mode that the native hardware was set to at the time that VSA connected to it.
The "CAL?" trace indicator message will show if a calibration is required, see CAL? Trace Indicator Messages help.
See Also