Quick Cal (Keysight X-Series Signal Analyzer configuration only)
selected
only applies to 89600 VSA system configurations that use an Keysight X-Series Signal Analyzer, see Keysight X-Series Signal Analyzer with 89600-Series Software. Selecting will initiate a smart calibration procedure. The calibration process only performs an alignment on sections that need re-alignment. is faster than a full and when completed, the entire instrument is aligned and calibrated.
When the property is selected, a is performed whenever the VSA determines that the hardware needs to be re-calibrated. Which sections are considered to need re-alignment is determined by the selected Calibration Mode.
See Also