Auto Calibrate (Calibration)
(Keysight X-Series Signal Analyzer configuration only)
Default: Cleared
only applies to the 89600 VSA system configurations that use an Keysight X-Series Signal Analyzer, see About Keysight X-Series Signal Analyzers with 89600-Series Software. When is selected, the VSA monitors the calibration status and automatically performs a Quick Cal whenever a calibration is needed.
can affect cumulative types of measurements where phase is important, for example time averaging. In these cases, can be turned off (cleared).
See Also