Actual Length (Gate Trigger)
(Power Spectrum based Input Domain Power Spectrum measurements only)
Displays the actual length of time in seconds of the acquisition data acquired and used for a step in the spectrum once the gate trigger condition occurs. This may be different from the desired Length parameter if the current resolution bandwidth cannot achieve the specific Length value (in which case the actual length used will be what is needed to achieve the resolution bandwidth).
See Also