Holdoff Style (Playback Trigger)
can be set for these playback trigger styles:
Playback Trigger parameters (including this one) affect the outcome of the time record when making a measurement.
There are two playback trigger that determine how the trigger Holdoff is defined:
- - Trigger specifies an amount of time that the recorded signal must be a stable low value (below the trigger level) before the next trigger can occur.
- - Trigger specifies an amount of time that the recorded signal must be a stable high value (above the trigger level) before the next trigger can occur.
See Holdoff for more details.
See Also