About Playback Triggering (Acquisition)
allows you to capture a block of time data around a particular event like hardware-based Trigger, but when playing recorded data.
See Playback Trigger Tab for parameter descriptions.
Trigger
The first parameter to select when setting up your trigger is the trigger Style. This determines the source of your trigger event (e.g. free run, channel, magnitude, periodic).
Playback Trigger and Segmented Recordings
Note the following when using Playback Trigger with Segmented Recordings:
- Only the first segment is triggered. Data from the remaining segments is taken starting at the same offset within the segment as the trigger offset of the first segment.
- When the trigger is found too close to the end of the segment such that the amount of data needed for a measurement update would cross the segment boundary, the trigger search routine will skip that trigger and start searching at the beginning of the next segment.
See Also