Playback Trigger Tab (Acquisition)
The tab sets up a trigger signal.
-
Playback Trigger Channel: Selects which input channel to trigger on.
Only one channel can be used to trigger the measurement.
-
Style: Determines the trigger type and trigger signal.
-
Delay (Segmented Capture = Disabled): Determines the amount of time used for trigger delay. When Segmented Capture is enabled,
-
Level: Sets the trigger level.
-
Slope: Sets the trigger slope.
-
Hold-off Style: Sets the trigger hold-off style.
-
Hold-off: Determines the amount of time used for trigger hold-off.
-
Periodic Trigger parameters: These parameters are used to set up and control the Periodic trigger style.
-
Period: Specifies the trigger interval.
-
Period Offset: Adds an offset relative to the periodic triggering point.
-
Sync Source: Determines how the first measurement is triggered.
-
-
Time Reference (t=0): Sets the time reference for playback.
-
Display Ref Line on Active Trace: Determines whether the trigger reference line is shown on the currently selected trace.
See Also