Style (Playback Trigger)

Playback trigger Styles contains a subset of the same trigger styles available when triggering from hardware.

Playback Trigger is unavailable for Power Spectrum measurements.

The type of playback trigger styles are described in the following list. For more details, click the name of the trigger type:

See Also

Playback Trigger Tab

About Playback Trigger

Acquisition menu