Gate Style (Acquisition)

If a particular trigger style is not available in the dropdown menu, it is because the measurement hardware or the trigger mode does not support that trigger style.

Unavailable trigger styles are greyed in the menu and cannot be selected.

Gated triggering is used in segmented capture (Segmented Capture = Enabled) and variable length segmented capture (Segmented Capture = Enabled and Segment Type = Variable) measurements. The available trigger gate styles are described in the following list.

For more details, click the name of the trigger type:

†Only one of these trigger styles is available at a time. The one that is available depends on instrument configuration, as shown in the table below.

Trigger parameters (including this one) affect the outcome of the time record capture from hardware when creating a recording as well as when making a measurement.

Only one of these trigger styles is available at a time: Channel Mag, IF Mag, and Magnitude. This table shows when each will be available.

Trigger style:

When available:

Channel Mag

When the input channel is I+jQ (ch1+j*ch2) and using two-channel hardware for which only the I or Q part of the signal can be used as a trigger.

IF Mag

When the time data is zoomed. 

Magnitude

When the logical input channel is an I+jQ channel and triggering on magnitude(I+jQ) is supported, or when the time data is baseband (real).

For information on triggering for specific measurement hardware, see Available Measurement Hardware .

See Also

About Trigger

Acquisition menu