Ref Offset (ACP Marker Properties)
specifies the frequency offset of the ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. measurement reference channel with respect to the VSA's center frequency.
See Also