Zero Delta
moves the reference marker for the selected delta marker to the position of the delta marker.
When is clicked and the active marker is not a delta marker, the VSA will change the active marker type to , add a new marker to the trace, and set the marker as the reference for the active marker, which is now a delta marker. Then the reference marker will be moved to the same location as the active marker. When band power is enabled for the active marker, the reference marker is set to be a normal marker with band power enabled and the band span is set to the same value as the active marker. When band power is not enabled for the active marker, the reference marker is set to be a fixed marker.
Right-click a trace grid and can be selected from the menu.
See Also