Moving Spectrogram Markers

When the spectrogram markers are enabled (see Selecting Spectrogram Markers) the easiest way to move the markers is with your mouse. Move the time or x-axis component of the marker by clicking and dragging the vertical or horizontal marker lines with your mouse. The mouse pointer changes to a bi-directional arrow («) to show that it is close enough to click and drag the marker.

Markers can also be positioned using the controls in the Markers Position tab by clicking Marker > Position and specifying the marker's X, Y, Z, and Trace Time position.

When a delta marker is selected, click Marker > Copy Marker to > Copy Markers to X Scale to copy the delta marker's X position and the reference marker's X position to the X-Scale left and right reference values.

The Y-position for fixed markers remains fixed when moving the marker with the mouse. Change the Y-position of a fixed marker by:

See Also

About Spectrograms (Spectrograms / 3D Map)

Copying Markers to

Position tab (Markers)

About Spectrogram Markers