Fast Averaging (Averaging)
When is on, the VSA updates the display after the number of averages specified by the Update Rate selection. This may increase measurement speed. For example, if an update rate of 5 is specified, the VSA updates the display after each 5 averages.
The Same as Count check box can be selected to set the update rate to be the same as the average count.
See Also