Update Rate (Averaging)
The setting of only affects fast averaging. The number entered in this field determines how often the VSA updates the display. For example, when an update rate of 5 is specified, the VSA updates the display once every 5 averages. The more often the display updates, the slower the measurement proceeds.
Same as Count can be used to set the update rate to match the average count.
See Also