Max Analysis Points (Frequency vs. Time)
Max Analysis Points represents an upper bound where analysis stops after exceeding this bound. Data will stop being processed beyond the max analysis point sample, and the rest of the data seen in the heatmap will be 0s. This can be increased or decreased, but increasing this could lead to a slow down in the VSA measurement.
When Auto is selected (default = selected), the max analysis points value is determined to be a reasonable starting place for all types of hardware.
Max Analysis Duration displays a read-only value to help customer understand what Max Analysis Points equates to in time.
See Also