ResBW (Frequency vs. Time)

ResBW sets the resolution bandwidth for Frequency vs. Time analysis measurements. ResBW in the Frequency vs. Time tab is not the same as the Analysis > ResBW > ResBW parameter. ENBW (Equivalent Noise Bandwidth)/ResBW is used to determine by how much time to split the capture time domain data into different slices before performing FFTs. For the Freq v Time Heatmap trace, these slices are then stacked on top of each other to achieve a heatmap perspective.

When Auto is selected (default = selected), the ResBW length is determined based on a factor of the Span of the measurement. This auto checkbox is not intended to provide the ideal ResBW, but a reasonable starting place for all types of hardware. At any point, if you change the ResBW value, auto will become unchecked.

See Also

Frequency vs. Time Tab

About Frequency vs. Time