Band Power Calculation (Markers)
Marker band power or power density can be shown as an average or a RMS (root mean square) value.
When is set to , the band power (or power density) is calculated as the average power in the band between the left and right edges of the band power marker.
When is set to , the average band power (or power density) is calculated and then the square root is taken.
See Also