Consolidate when Code Order is Hadamard (Markers)

(WCDMA(3GPP) and cdma2000 demodulation only)

The Consolidate when Code Order is Hadamard check box controls the Code Domain Power trace data marker placement. When the check box is checked, markers are placed on all related code channels (Walsh Code Number). When the check box is cleared, a marker is placed only on the selected code channel (Walsh Code Number).

The code channels can also be reordered so that all related channels are placed adjacent to each other by setting the Code Order to Bit Reverse (click Trace > Properties > Digital Demod > Code Order and select Bit Reverse).

See Also

Position Tab (Markers)

About Ch1 CDP Trace Data (cdma2000/1xEV-DV)

Antenna (x) CDP and Antenna (x) Trace Data (W-CDMA(3GPP)/HSPA)