Bus Name (Digital Input)
provides all the Logic Analyzer data bus names available for the selected input module or software Tool. Select the bus or buses used as data inputs by the 89600 VSA software. The description of the Parts property describes how the data from the selected buses are mapped.
For data streams composed of two data Parts (I/Q or Magnitude/Phase), there is a drop down list for each .
The property is channel specific.
See Also