Frequency (Digital Input)

Menu Path:Acquisition > Digital

The Frequency group specifies the Sample Rate and Center Frequency associated with the data stream coming from the Logic Analyzer. These must be set to allow proper scaling of both time and frequency displays. They also establish the limits for the measurement Center Frequency and Span.

The Sample Rate and Center Frequency properties are channel independent and are applied to all channels (Digital Channel is ignored).

See Also

About Digital Input Properties

Composition

Data