Data (Digital Input)

Menu Path: Acquisition > Digital

Digital Data from a Logic Analyzer can be interpreted as signed data in two ways, two's complement or offset binary. The Sign and Scale data properties specify the data Sign convention and the Scale factor for each data part. The Scale property is channel specific but the Sign properties is channel independent.

See Also

About Digital Input Properties

Frequency

Composition