Preset Measurement to Defaults

Clicking File > Preset > Measurement to Defaults will configure the selected measurement's properties to their default states. Selecting Preset Measurement to Defaults will not affect the trace layout or most of the parameters under the Acquisition, Markers, and Analysis menus (except for those in the <Measurement Type> Properties... dialog).

This menu item is only available with certain measurement types (e.g., Component Test).

See Also

Preset Setup

About Preset