Preset Measurement to Standard
Clicking and choosing a standard preset will configure the selected measurement's settings to demodulate the selected preset.
This menu item only shows the standards supported by the currently selected Measurement Type.
Each demodulator provides certain presets that can be used to demodulate signals that follow a known standard. These demodulator presets are also available from the tab of the dialog by clicking the button.
Details for these presets are listed in the Making Measurements book in the Table of Contents for a demodulator in the Using Standard Presets topic. To quickly get to the documentation for a demodulator, see the Selecting a Measurement Type topic.
See Also