X Axis Format and Y Axis Format (Trace Format)
(applies only to Real vs. Imag trace format)
and set the coordinate transform for the x and y axes, respectively. These parameters are only available for the Real vs. Imag trace format.
These are the coordinate transforms that are available:
- - the coordinate of a point is untransformed (positive and negative values are preserved).
- - the magnitude of a point is plotted in linear units
- - the magnitude of a point is plotted in logarithmic units
See the Real vs. Imag topic for more information.
See Also