Reference Level (X Scale)
(applies only to Real vs. Imag trace format)
sets the value of the invisible, vertical reference line (for example, 0 dB) and Reference Position sets the position of the reference line within the trace viewport.
See Also
(applies only to Real vs. Imag trace format)
sets the value of the invisible, vertical reference line (for example, 0 dB) and Reference Position sets the position of the reference line within the trace viewport.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |