X Scale Tab (Trace)
The X Scale tab sets the X-axis scaling and positioning of data displayed in the active trace.
- Trace controls: At the top of the tab are controls for selecting, adding, and removing traces.
- :
Select the check box to make the trace visible on the display; clear the check box to remove the trace from the display. When the trace is selected, the following parameters can be set for the trace:
For all trace formats except :
- Full Scale determines how much of the trace data is shown.
- Left Reference sets the value for the first point displayed.
- Right Reference sets the value for the last point displayed.
- Show Frequency Center/Span on all traces determines whether Center/Span or Start/Stop frequencies are shown below each frequency domain trace.
For the Real vs. Imag trace format:
To quickly reset the x-axis to full scale: Right click in the x-axis annotation area of a trace (below the trace grid) and select .
See Also