Y Per Division / Y Ratio (Y Scale)
The name of this parameter changes between and , depending on the Y-axis format. For , the parameter is . For all other formats, the parameter is .
defines the spacing between vertical divisions (denoted by graticule lines when Show Grid Lines is enabled). Increase to show more data in the trace grid (and reduce the resolution); decrease to show less data in the trace grid (and increase the resolution).
can be changes by clicking that hotspot in the trace window.
is used for the trace format the ratio of top of the trace grid to the bottom of the grid (ratio of Y Top to Y Bottom). For example, if CCDF Complementary Cumulative Distribution Function is displayed with a Y Top of 100% and a Y Bottom of 1%, the is 100.
See Also