IF Calibration File (User Correction)

Menu Path: Acquisition > User Correction

IF Calibration File is the stored measured frequency response of the device IF Filter compensates for. The image\ellipsis.jpg button next to the IF Calibration File field provides the means to browse for a file created previously.

For details on how to generate the file, see User calibration file format. The name of the file and the directory it is stored in are unrestricted.

See Also

IF Filter

About User Correction