Data Power Analysis (802.15.4 HRP UWB)
enables analysis of the data portion of the frame (PHR+PSDU 1) PHY Service Data Unit, or 2) PLCP SDU). The demod will try to analyze the data portion of the frame and calculate the power metrics in the Syms/Errs trace. The minimum Search Length will be set to capture the data, but if not possible (e.g., the recording is too short), then the data metrics will not be calculated.
Default: Disabled
See Also