IEEE 802.15.4 HRP UWB Demod Properties Dialog Box

Menu Path: Analysis > IEEE 802.15.4 HRP UWB Demod Properties

The IEEE 802.15.4 HRP UWB Demod Properties dialog box contains parameters that let you configure the VSA to demodulate 802.15.4 HRP UWB signals.

The 802.15.4 HRP UWB demodulator must be selected before this dialog box is available. To enable the demodulator, click Analysis > Measurement Type > Wireless Connectivity > IEEE 802.15.4 HRP UWB

The IEEE 802.15.4 HRP UWB Demod Properties dialog box contains tab headings that group similar configuration parameters as follows:

See Also

About IEEE 802.15.4 HRP UWB