Format Tab (802.15.4 HRP UWB)
The tab of the IEEE 802.15.4 HRP UWB Demod Properties dialog box provides parameters to configure the 802.15.4 HRP UWB signal for analysis.
Below is a list of the parameters in the tab:
- Hop Bursts
- Chips per Burst
- Constraint Length
- Data Rate
- Frame Length (Octets)
- FCS Type
- Decoding Level
- Segment Length (x512 chips)
- Number of Segments
- Extra Gap (x4 chips)
- Key (128 bits)
- Upper Part of V (96 bits)
- Initial Count (32 bits)
- Number of RIFs
- Segment Length (x512 chips)
- Add 1ms Gap between RSFs and RIFs
- Key (128 bits)
- Upper Part of V (96 bits)
- Initial Count (32 bits)
See Also