STS Packet Configuration (802.15.4 HRP UWB)
When an ERDEV PHY Mode is selected (ERDEV-BPRF or ERDEV-HPRF), selects the scrambled timestamp sequence (STS) configuration mode. This setting determines the presence and location of the STS within the frame.
No STS (0)- STS is not present in the frame.
After SFD Start frame delimiter (1)- STS is located after the synchronization header's SFD and before the PHR.
After PHR/Payload (2)- STS is located after the PHR/Payload at the end of the frame.
After SFD, no data (3)- STS is located after the synchronization header's SFD. The frame does not contain PHR/Payload data.
Default: No STS (0)
Choices: No STS (0); After SFD (1); After PHR/Payload (2); After SFD, no data (3)
See Also