Time Tab (802.15.4 HRP UWB)

Menu Path: Analysis > IEEE 802.15.4 HRP UWB Demod Properties... > Time tab

The Time tab of the IEEE 802.15.4 HRP UWB Demod Properties dialog box lets you access the signal capture configuration parameters. You use these parameters to isolate a portion of the time record (captured input signal) for further viewing and data analysis.

The Time tab lets you configure these parameters (click on the parameter name for further information):

See Also

Advanced Tab

Format Tab

IEEE 802.15.4 HRP UWB Demod Properties Dialog Box