Main Lobe Pk (802.15.4 HRP UWB)
is the peak height of main lobe, expressed in percent (100% = 1.0 on the RRC Correlated trace).
The main lobe and side lobe metrics are computed from the RRC Correlated trace.
See Also
is the peak height of main lobe, expressed in percent (100% = 1.0 on the RRC Correlated trace).
The main lobe and side lobe metrics are computed from the RRC Correlated trace.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |