RRC Correlated (802.15.4 HRP UWB)
The trace shows the cross-correlation between the measured UWB pulse and a root raised cosine (RRC) pulse. The RRC pulse has a 3 dB bandwidth as defined in Table 16-11 of the standard for the selected Channel.
To calculate this trace, the impulse response is correlated with the RRC pulse and normalized by the energy of the reference and measured impulse response so that a value of one indicates perfect correlation.
The Min Main Lobe Width, Max Side Lobe, Side Lobe Pk and Side Lobe Pk Loc metrics are computed from this trace.
See Also