Main Lobe Width (802.15.4 HRP UWB)
is the width of the main (center) lobe that is above 0.8.
The main lobe and side lobe metrics are computed from the RRC Correlated trace. The resulting cross-correlation magnitude of the main lobe should be ≥ 0.8 for at least Tw (main lobe width, see Table 16-12 of the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.15.4 standard).
See Also