Max Side Lobe (802.15.4 HRP UWB)
indicates PASS/FAIL of the maximum sidelobe height requirement, as specified in the standard. The largest sidelobe should be ≤ 0.3. See the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.15.4 standard document for more information.
The main lobe and side lobe metrics are computed from the RRC Correlated trace.
See Also