Min Main Lobe Width (802.15.4 HRP UWB)
indicates PASS/FAIL of the minimum main lobe width requirement, as specified in the standard. The resulting cross-correlation magnitude of the main lobe should be ≥ 0.8 for at least Tw (main lobe width, see Table 16-12 of the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.15.4 standard).
The main lobe and side lobe metrics are computed from the RRC Correlated trace.
See Also