Side Lobe Pk (802.15.4 HRP UWB)
is the peak value of highest sidelobe relative to the main lobe.
The main lobe and side lobe metrics are computed from the RRC Correlated trace. The largest sidelobe should be ≤ 0.3. See the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.15.4 standard document for more information.
See Also