Side Lobe Pk Loc (802.15.4 HRP UWB)

Side Lobe Pk Loc is the offset from the main lobe peak location.

The main lobe and side lobe metrics are computed from the RRC Correlated trace.

The Side Lobe Pk Loc data is internally resampled to a higher sample rate to determine the location displayed in the Syms/Errs summary table, providing more time resolution than may be observed from a marker on the RRC Correlated trace.

See Also

Available Error Summary Data