Search Time (802.15.4 HRP UWB)
shows the time record data after resampling and time adjustment. The time scale of is shifted such that 0 ms corresponds to the beginning of the 802.15.4 HRP UWB frame.
The next step is to locate the frame within the data and place this data into the Time trace.
Time (shown in the diagram below) will contain the part of the frame that is demodulated (which depends on the parameters).
See Also