Time (802.15.4 HRP UWB)
The trace contains the data (SHR) used in calculating Demod traces.
Time (shown in the diagram below) will contain the part of the frame that is demodulated (which depends on the parameters).
See Also