Keysight PathWave License Manager
The Keysight PathWave License Manager (PLM) is required when using floating or USB portable licenses. The PathWave License Manager enables you to connect to a license server (e.g., Keysight License Server) and manage the licenses for your VSA software.
The PathWave License Manager is installed separately from the VSA software. If the Keysight PathWave License Manager is not already installed, you can download it at http://www.keysight.com/find/plm.
The Keysight PathWave License Manager is a stand-alone application with its own help system. If the Keysight PathWave License Manager is installed, you can launch it from the Start menu or by clicking Keysight PathWave License Manager... within the VSA software. Refer to the PathWave License Manager's help system for more information.
See Also