Setting Up a Client PC
When floating or USB portable licenses are used, the client PC or instrument requests a license from the server to run the 89600 VSA software. If a license is available, the server will allocate the license to the client. A client PC needs to be properly configured to communicate with the license server and the VSA software.
The PathWave License Manager (PLM) is required when using floating or USB portable licenses.
To set up a client PC:
-
Launch the PathWave License Manager (installed with the VSA software).
-
Add (install) license files. See the PLM help system for detailed steps.
-
Specify a remote license server. See the PLM help system for detailed steps.
See Also