Obtaining a Trial License

To obtain a trial license, follow these steps:

  1. Obtain the license Host ID (Model Number, Serial Number) from the PC that you installed the VSA software on.
    1. Launch the Keysight Software Manager Utility. Within the VSA software, click Utilities > Licenses > Status > Keysight Software Manager Utility..., or from the Windows desktop, click Start > Keysight Software Manager Utility.
    2. Copy the Keysight Host ID at the top of the Add License tab.

    3. For Measurement Hardware (instruments), the Keysight Host IDs consist of an Keysight instrument model number and serial number. On a desktop or laptop PC, the default model number is PCSERNO.

  2. Go to the Keysight 89601B VSA website at www.keysight.com/find/89601B, select the Software & Trials tab, then follow the instructions to obtain a trial license.
  3. After you finish using the Keysight Software Licensing website, check your email for your license file, then go to Installing a Trial License.

See Also

Trial License Overview

Keysight Software Manager Utility